9/23/2022 1:34 PM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, When running OS Project Editor, you have a few tabs like Basic Data you already mentioned. When the checkmark is set (by default), the OS project editor will update the pictures with the pictures installed on the PC station. If you have changed the pictures in the project, those changes are lost. You can prevent this by copying the customized pictures also to the PC station folders-> Siemens\WinCC and place them in the correct folders. When the checkmark is not enabled, OS project editor will not update the pictures with the pictures from the library. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on