12/23/2008 9:15 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Dear z0de, I think you could use SFC51 to read information about the system. See this manual: http://support.automation.siemens.com/WW/view/en/1214574 Chapter 13.3 will explain the function. Then you can use Simatic Net (OPC server) to get data out of the CPU into a PC. And Excel might be an OPC client. With Visual Basic you can put data on the right place. See this link: http://support.automation.siemens.com/WW/view/en/15355168 Perhaps these links are useful: http://support.automation.siemens.com/WW/view/en/24299099 http://support.automation.siemens.com/WW/view/en/23931842 Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
12/23/2008 4:35 PM | |
Posts: 3 Rating:
|
Good information, I am actually using Borland Delphi for the interface, which is very similar to VB. If i have any questions I'll be sure to come back here. |
12/24/2008 9:10 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Dear z0de, |
Last edited by: Wizard at: 12/24/2008 9:12 AMadding text |
|
Follow us on