5/31/2019 9:38 AM | |
Posts: 4 Rating:
|
Hello, Did you finally succedd on establish the connection between the S7300 CPU and S7-1200 CM1242? I am configuring the HW and SW and I have doubs regarding how to programm the data exchange (I am using FB15 PUT) because I would want to send 750 bytes. How many slots should I configure in the HW configuration of CM1242 module? I have configure 64 Word inpunt and 64 word output. Any help?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/31/2019 12:46:58New subject after splitting |
|
5/31/2019 1:50 PM | |
Joined: 9/27/2006 Last visit: 9/13/2025 Posts: 12408 Rating:
|
Hello sergio; To help us understand your situation, could you show or describe o us your present configuration between the S7-1200 and the S7-300? We can provide as much help as we can, as long as we have good information on your problem. In the meantime, this FAQ discusses Put/Get between a s7-300 and a S7-1200. How do you configure and program an S7 connection and the FB15 'PUT' and FB14 'GET' function blocks for data transfer between an S7-1200 CPU and an S7-300 CPU?H https://support.industry.siemens.com/cs/ww/en/view/92269951 Study the pdf included in the downloads, and understand that with Put and Get you must establish an unilateral connection between the 2 CPUs. That means: only one of the CPUs specifies a connection, the other partner is marked as Unknown. The functions Put and Get are generated only in the active partner (the one with the established connection). Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 05/31/2019 16:10:49 |
|
Follow us on