3/9/2019 3:04 AM | |
Posts: 17 Rating:
|
Hello I can control how many axis kinematic 6ES7 511-1TK01-0AB0 |
3/9/2019 11:41 AM | |
Posts: 17 Rating:
|
Hello I think the problem is improving when I replace it with a CPU 1515T-1 PN 1511T-1 Not suitable for doing this job Thank you |
3/11/2019 2:09 PM | |
Joined: 4/28/2015 Last visit: 8/7/2025 Posts: 399 Rating:
|
Hello, you have to check the available Motion Control resources of your CPU: S7-1511T (see: Technical data)
Then you have to calculate... But what ever, it will be only one kinematics with S7-1511T... :-) |
This contribution was helpful to
1 thankful Users |
3/11/2019 4:13 PM | |
Joined: 10/11/2006 Last visit: 8/29/2025 Posts: 6037 Rating:
|
Hello, without dynamic adaption, it is possible to reduce the load. 3.9.3 Motion dynamics Dynamic adaptation https://support.industry.siemens.com/cs/ww/en/view/109749264 The configured setting in "Technology object > Configuration > Extended parameters > Dynamic" is used. (<TO>.DynamicDefaults.Dynamic- Adaption) and with less commands in the queue: A.1.9 Tag MotionQueue (kinematics) The tag structure <TO>.MotionQueue.<tag name> contains the configuration of the job sequence parameters. MotionQueue.MaxNumberOfCommands Maximum number of jobs in the job sequence (configuration is performed using the parameter view (data structure)) |
With best regards, |
|
This contribution was helpful to
1 thankful Users |
3/12/2019 2:23 PM | |
Posts: 17 Rating:
|
Hello there Can you open the issue a little more thank you in advance for your support
|
Follow us on