4/22/2022 6:18 PM | |
Joined: 2/25/2020 Last visit: 8/3/2024 Posts: 4 Rating:
|
hi everyone, I am trying to achieve communication between two s7-1500 systems located in two different stations, as per attached architecture using SCALANCE M876-4 using SIM cards with Static IPs. I am able to ping the station 1 Sim card external static IP address and internal LAN IP address from station 2 Web management "Ping" option and vice versa. But i am unable to ping the devices on either side of the internal LAN from both station. did any one faced such issue? i tried NATMAP setting as per manual as well as port forwarding but nothing works. I have allowed everything in the firewall as well. Edit: in architecture i have mentioned Scalance M874-2 but i am using Scalance M876-4 physically.
AttachmentARCHITECTURE.pptx (669 Downloads) |
Last edited by: rosshan at: 04/22/2022 18:20:53 |
|
12/27/2023 10:47 AM | |
Joined: 10/11/2023 Last visit: 3/31/2025 Posts: 2 Rating:
|
Dear rosshan, Can you show prints of the configuration you made on the m876? and at TIA Thank you. Best regards |
Follow us on