5/22/2024 10:26 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Setting an SFC to auto is not possible via batch. What you can do is creating a tagcollect value which connects to the QAUTMAN (1=SFC in auto, 0=SFC in manual) and use the value as transition in the batch recipe before the EPH should be started. But in general when I need to have an equipment set to manual, in our terms it means that the batch is suspicies and our customers won't accept that. You can always create logic to put the SFC to automatic mode like in IDLE sequencer.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on