1/28/2017 5:56 AM | |
Posts: 17 Rating:
|
Dear all, hello. My system is simoution D425-2 DP/PN, CU320-2 with sinamics S120. I want to connect my PC to it for upload project. It is mentioned that before I installed the simoution scout v4.3 and get the communication between simoution D425. Communication between simotion and PC by profibus adapter, as well as tried connection and through profinet.
In both events possible upload only HW configuration D425-2. There are nodes with question mark after selection scaning of the accessible nodes. I cannot fully upload my system. Please help me in order solving this problem. How step by step make unloading the project? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/30/2017 10:21:57 AMNew subject after splitting |
|
1/30/2017 8:09 AM | |
Posts: 17 Rating:
|
Thank Christoph that responded. |
1/30/2017 10:49 AM | |
Posts: 17 Rating:
|
You want to say that starter from scout v 4.3 no need to change the starter on the v 4.5? I wanted to upload Simotion Data like Programs and Technology Object. |
2/1/2017 7:56 AM | |||
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, 1.) You have no CU320-2 DP/PN ! And Simotion D425-2 DP/PN is not supported in STARTER, here you can't upload any Simotion Data!
" Regards |
||
Follow us on