1/20/2007 8:24 PM | |
Posts: 2 Rating:
|
How can I get the Gsd file of "sm 326" fail safe I/O module? |
1/21/2007 11:46 AM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Dear Abbas, There is no GSD-file for the SM326 Failsafe In- and Outputs. Normally this SM 326 are coming with Distributed Safety or with F-System, there the librarys are installed and also the hardware that could be used for the Version you have. You may download: Download of the F Configuration Packso that the Failsafe I/O comes in the librarys. Please consider that this one is not the newest (V5.5 is the newest and comes with the F-System or with DS) configurationpack. You need also Distributed Safety or F-Systems to program theFailsafe I/O, but with the Configuration Pack you see the modules in your hardware. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on