4/3/2023 2:07 PM | |
Joined: 10/6/2022 Last visit: 1/31/2025 Posts: 60 Rating:
|
Hello! In this document: How do you do a SIMATIC HMI operating system update (firmware update, OS update) o... - ID: 19701610 - Industry Support Siemens there is a PDF: 19701610_prosave_1_2_e.pdf Start ProSave via "Start > SIMATIC > ProSave > ProSave".
• In the ProSave menu bar you select the General menu and define the device
type. The last step is not true. There is no image by default. However; I can manually select an image, but this image does not appear to match my device. "The connected device does not match the selected file". Since there is only one image to choose from when it comes to TP177A I'm assuming I must have done something wrong. Perhaps my adapter is not able to connect to my device. |
Last edited by: Jen_Moderator at: 04/04/2023 09:22:31Link optimized. |
|
4/4/2023 11:01 AM | |
Joined: 7/19/2022 Last visit: 9/8/2025 Posts: 436 Rating:
|
Hello Figuren, To reset to factory settings you must check the box that says "Reset to factory settings" in the OS Update section. |
If this Information really helps, you could use the Rate function |
|
Follow us on