12/7/2011 9:41 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello Johncmpa, sadly this isn`t possible. You can do a backup of your OP77A programm, but this can also just restored to a OP77A. A backup can´t be edited, he can just restored in the same type of device. For example: Backup OP77A -> Restore OP77A, possible Backup OP77B -> Restore OP77B, possible Backup OP77A -> Restore OP77B, not possible The back transfer of a project is possible, but to do this you have to activate this option at the first download of the project (i think this isn`t done in your case). If this option isn`t activated you can just work with ProSave and the backup/restore function. Take a look at these FAQs to understand the differenz between backup/restore and a back transfer. How do you backup/restore with a Windows-based panel? How do you back transfer the projects of an operator panel and what should you watch out for? best regards |
This contribution was helpful to
1 thankful Users |
12/7/2011 12:18 PM | |
Joined: 10/2/2008 Last visit: 12/15/2023 Posts: 5 Rating:
|
OK, thanks for the information, that's all I wanted to know. Thanks again |
Follow us on