7/7/2010 11:00 AM | |
Posts: 3609 Rating:
|
Import of a Technical Question of an User alexcontrolwrote: Hello friends, I'm new using Micromaster Profibus dp interface. I have a PLC cpu 315-2DP and the MM420 and as you know I´m goning to connect the two devices using PROFIBUS DP communication what I want to know is how to control the MM420 with step 7 software (configuring the hardware, creating the kop program with common libraries) |
7/7/2010 11:06 AM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi Alex, Please Have a look on the Following FAQ MICROMASTER 4 & SINAMICS G Function block (FC14) to control an MM4 via Profibus-DP Directly controlling a MICROMASTER 4 / SINAMICS G120 / SINAMICS G120D from a SIMATIC HMI station via PROFIBUS-DP and PROFINET Enjoy .... |
Ammy |
|
This contribution was helpful to
1 thankful Users |
7/7/2010 4:45 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
As you are new, here are some more links of threads related to Profibus Communication... |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on