4/2/2025 9:13 AM | |
Joined: 9/30/2016 Last visit: 9/16/2025 Posts: 947 Rating:
|
Please also see the attached screenshots. I need to make some modifications to a machine. Now I need to connect to the basic panel with TIA V18 and download the modifications to the panel. When I try to search for the panel (or any available components) with TIA it does not find anything at all. Is there a PG/PC setting in TIA (different from the setting that just worked in Simatic Manager) that I need to set or what am I doing wrong? AttachmentOnline 1.zip (335 Downloads) |
4/3/2025 10:42 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello xmnj, Try the following: and type the IP Address of your panel Best regards, Wizard |
4/7/2025 6:02 AM | |
Joined: 9/30/2016 Last visit: 9/16/2025 Posts: 947 Rating:
|
Hello again Hati, Please also see the attached screenshots. Unfortunately it doesn't seem to be working. I found an USB stick and dragged and dropped the HMI to the USB memory. I checked on the stick and it has created a folder called "Simatic_HMI". In this folder there are 2 folders: "Firmware" and "RT_Projects". I found a (brand new and empty) panel in our spare parts and powered it up. I inserted the USB stick and went to the restore section on the panel. It found the USB stick but when I go to step 2 it does not find any archive files. What am I doing wrong and how can I make this (workaround) work?
AttachmentUSB DL.zip (307 Downloads) |
4/7/2025 6:49 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hi, Please have a look at the following link: Transfer HMI project offline to operator panel Best regards, Wizard |
Follow us on