2/16/2021 8:41 AM | |
Joined: 8/21/2014 Last visit: 7/31/2025 Posts: 142 Rating:
|
What is the difference between _runVelocityBasedMotionIn and _runPositionBasedMotionIn? If iam using _runVelocityBasedMotionIn for coupling will the slave axis follow the position of master?. In our case both master and slave are real Linear axes. We want to home this axis(moving to a external homing sensor). If we are using _runPositionBasedMotionIn the slave will move rapidly at the position setting stage of homing(At the end of homing of master the current position of master will set to zero.) If we are using _runPositionBasedMotionIn, then the slave rapid movement is not there. But the confusion is will the slave follow position of master or not? We want a gearing on position. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/16/2021 12:30:49New subject after splitting |
|
Follow us on