6/19/2017 5:40 AM | |
Joined: 1/25/2010 Last visit: 8/29/2025 Posts: 11 Rating:
|
Hi Oreca, May I know what kind of PCS7 license do I need to add in my Engineering Station if I would like to use CMT? It seen like I would need Version Cross Manager in order to do the synchronization of CM. Thanks & Regards, Chia WC ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/21/2017 10:25:54 AMNew subject after splitting |
|
6/20/2017 7:49 AM | |
Joined: 3/14/2008 Last visit: 9/3/2025 Posts: 2216 Rating:
|
Hi, You won't need Version Cross Manager license. You need the following license: 6ES7658-1GX08-2YA5 This is a license for Advanced ES software, which is supplied with the DVD Software Media Package for PCS7 V8.0 and (not sure) V8.1. You must install this software in order to synchronize Control Module Types to instances. Another way is to use the software COMOS, but this will require knowledge of the software. Advanced ES is a small portion software, taken from COMOS and modified for easy use. You can download updates from the following link: |
Last edited by: Oreca at: 6/20/2017 7:55:15 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on