6/26/2025 7:20 AM | |
Joined: 1/21/2013 Last visit: 9/11/2025 Posts: 4102 Rating:
|
Hi George, As the ordering data list included with the WinCC Unified V20 delivery release shows, the 6AV2155-2FS02-4LA0 starter package contains the following ordering numbers:
Yes, as long as the price stays the same, you will get four software packages for free. That's a 30% discount! Kind regards |
This contribution was helpful to
1 thankful Users |
6/26/2025 8:35 AM | |
Joined: 8/1/2012 Last visit: 9/10/2025 Posts: 17 Rating:
|
Hi Stefan, Thank you for the link I will have a read :-) Would those 1000 logging tags work alright with the SQL add-on? |
6/26/2025 9:36 AM | |
Joined: 1/21/2013 Last visit: 9/11/2025 Posts: 4102 Rating:
|
Hi George, Logging tags are licensed separately, regardless of whether file-based or database-based logging is used. For instance, the "WinCC Unified PC 1000 Logging Tags" license permits logging of up to 1,000 tags per license. In order for database-based logging to be used, a "WinCC Unified Database Storage" license will need to be purchased. For details, please refer to the licensing section of the user documentation. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on