7/14/2014 9:35 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello TechDiff, I recommend to install at first the actual Update 7 for WinCC V7.2. http://support.automation.siemens.com/WW/view/en/92023320 Maybe it solves the crash. If you would have the same problem with Update 7 too, you should create a manual userdump from "grafexe.exe" via Taskmanager. Then create a Service Request an send the userdump to the Technical Support. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to
1 thankful Users |
7/14/2014 12:08 PM | |
Posts: 17 Rating:
|
HelloGeorg , Thank you for your help , unfortunately I am still facing the same problem ... I'll send the dump file to technical support. Thanks again.
|
Follow us on