7/1/2021 6:15 PM | |
Joined: 9/3/2008 Last visit: 8/19/2025 Posts: 938 Rating:
|
Hello One thing that comes to mind is that you get an overview of the amount of data that is being logged in the Alarm and taglogging. WinCC can handle up to 200 database segments in total, so you need to configure the alarm and taglogging correctly so the size and number of segments does not exceed this. See: How many single segments can be connected to the SQL server in PCS 7 without impairing performance? and Why does the SIMATIC WinCC Runtime not start up or hang in the Start routine? Regards |
Michael |
|
Follow us on