8/24/2009 4:40 AM | |
Joined: 10/7/2005 Last visit: 9/2/2025 Posts: 3049 Rating:
|
Hello Waqas YES, this is possible. WinCC(as of version 6.x, not too sure which one exactly) does icludethe so called "Softnet Lean" license which allows for up to 8 connections. If you need more you'll have to purchase the "full" Softnet licensewhich allows forup to 64 connections (e.g. you could theoretically have one WinCC PC "talking" with 64 S7 PLC's)
The setupdepends on what type of connections (Ethernet, Profibus. MPI etc.) and is quite well explained in the Communication chapter of the WinCC information system (which you can find in the WinCC program group assuming you haveWinCC installed). I hope this helps |
Cheers |
|
Follow us on