7/12/2021 6:07 PM | |
Joined: 3/19/2010 Last visit: 6/15/2025 Posts: 439 Rating:
|
Hi, I have "successfully" installed Wincc/Audit 7.4 Update 2 on top of WinCC 7.4 SP1 Update 17, but it's icon doesn't appear in the WinCC Explorer. As if it didn't exist whatsoever (see pictures 1 and 2). -Inst. Software says: it is there! (see picture 3) If I try to repeat the installation, it says it is already installed. (see picture 4) Viewer is there, as a stand alone program. Installation went smoothly. OS is Windows Server 2016 Standard. NOTE: Absolutely identical situation on 2 identical servers. AttachmentAudit screens.zip (145 Downloads) |
Follow us on