12/6/2010 5:22 PM | |
Posts: 621 Rating:
|
dear friends and experts [schnippschnapp] A powerplant has 8 gensets operating in grid parallel mode. In one genset sometimes there is pf variation and kvar variation. The plant operates in pf mode. When this variation is observed the load is stable, voltage is also stable, freq and genset speed is also stable. How will you check the functioning of pf card. What shall be the ideal output vdc of the pfc, from there it is input to AVR? with best regards algudkar Splitted from Why all voltage level are multiples of 11, like 220V, 440V, 1100V instead of 200V, 400V, 1000V?. |
Last edited by: O_Moderator at: 12/8/2010 2:05 PMnew subject after spliting |
|
Follow us on