(2)| 12/6/2010 5:22 PM | |
|
Posts: 621 Rating:
|
dear friends and experts 1 - Why all voltage level are multiples of 11, like 220V, 440V, 1100V instead of 200V, 400V, 1000V? [schnippschnapp] the other questions are splitted to What is the direction of both Vibro Motors?. What shall be the ideal output vdc of the pfc, from there it is input to AVR?. with best regards algudkar |
Last edited by: O_Moderator at: 12/8/2010 2:04 PMnew subject |
|
Follow us on