(0)| 12/6/2010 5:22 PM | |
|
Posts: 621 Rating:
|
dear friends and experts [schnippschnapp] Two electrically operated Vibro Motors are fixed in parallel direction in vibrating feeder. What is the direction of both Vibro Motors? [schnipschnapp] with best regards algudkar Splitted from Why all voltage level are multiples of 11, like 220V, 440V, 1100V instead of 200V, 400V, 1000V?. |
Last edited by: O_Moderator at: 12/8/2010 2:05 PMnew subject after spliting |
|
Follow us on