1/24/2011 5:44 AM | |
Posts: 11 Rating:
|
Following the suggestions offered by KSN everything has worked out well (USS communication noe working well). Now there is another problem(s), the drive gives an error F024 (Encorder Error) it is an RA24 SIMOREG series drive. I have confirmed the encorder is OK by using the encorder on another drive. What is strange is that the enorder i use: EL40A000Z5/28P6X6PR2 is a 2000 pulse per rev, yet with this data, the drive gives F24 immediatelyyou start. if I use a fake setting of 500 pulse per rev, the drive runs for about 5 mins before giving the error F42. Further at low speeds the drive "cogs" i.e. behaves as if the movement is pulseting for a wile before the drive picks smooth run..... What is wrong??? Splitted from Simoreg 6RA70 Series and USS protocal. |
Last edited by: O_Moderator at: 1/25/2011 8:16 AMnew subject after splitting |
|
1/24/2011 7:51 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Manual SIMOREG K 6RA23 |
Follow us on