12/2/2024 1:57 PM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4108 Rating:
|
Hi SlamaMartin, It is difficult to answer a question with such a vague description. With WinCC Unified, you may be able to display the contents of the SD card file using the web server functionality. However, you will not be able to perform some actions on the files, such as reading, writing or deleting. This is because WinCC Unified scripting does not allow connections to other web servers. Depending on your system (PC Runtime or Unified Panel), you may be able to do what you want by using local scripts (bat files or bash scripts). Without using the PLC web server, you will not be able to access files on the memory card. Kind regards |
Follow us on