9/28/2016 7:16 AM | |
Posts: 3 Rating:
|
Hi, I connected IO device to the controller . The IO device is TI Evaluation Module(ICE AM3359) v2. The evaluation kit is running with PROFINET RT + MRP slave application. SIEMENS CP1616 is the IO controller. Am new to this environment can any body help me to create a simple project for CP1616 as PC Station and one simple IO device connected via PROFINET . Or any link or document for creating the project . I refer BA_CP1604-CP1616_76 and PH_PC-Stations_76 documents for creating project and downloading but facing issue as BF LED flashes. Kindly help me out to resolve the issue. I have attached the diagnostic buffer screen shot but not able to understand can any body tell me how to understand the diagnostic buffer messages. I have attached one document explaining the hardware setup and project details . Regards, Subeesh babu 8939229627 AttachmentSiemens-NCM-Manager-ProblemsFacing.docx (392 Downloads) |
10/3/2016 7:48 AM | |
Posts: 3 Rating:
|
Hi, Any help. Am stuck up with the issue which I posted earlier. Kindly help me by providing any valuable suggestion or solution . Thanks & regards, Subeesh |
Follow us on