3/11/2024 10:02 AM | |
Joined: 11/13/2023 Last visit: 2/4/2025 Posts: 1 Rating:
|
Hi I've been struggling for a while and feeling really stuck now, can't download to WinnCC Unified Runtime on PC via VPN. Pinging works, both devices appear both under "Accessible Devices" and "Online Access"... Just downloading to Runtime fails with "Failed to establish a connection to the device" It works great when connected locally to the IXON Router (either with cable or via WiFi), but not via VPN. Feels like the Ethernet type of PG/PC Interface called "HMI Ethernet" doesn't see or use the TAP-Windows V9 network adapter created by IXON. I couldn't even find the settings for this HMI Ethernet PG/PC interface to see if there are some weird settings there? Attachmentpictures.docx (416 Downloads) |
Follow us on