6/5/2013 3:30 AM | |
Posts: 17 Rating:
|
This is the ComProfibus file.
AttachmentFinal_06FEB13.zip (386 Downloads) |
6/5/2013 5:19 AM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
Hello little_tiger you've already declared I/O modules withParea I/O addresses for the IM308C DP Slave which prohibits you from changing to page addressing mode. Easiest way is to delete the whole S5 IM308C DP Slave station, add a new one and set the addressing mode first. One more thing, if only all your P area related addresses are used, you can stillstay with linear addressing mode and use the Q area address range instead (or alternativelyFB192 via thethe DP window if need be). Thechoice is yours and chapter 6.1 of the ET 200 Distributed I/O System with IM 308-C and S5-95U contains all the details and important info on what to consider. I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
6/5/2013 7:01 AM | |
Posts: 17 Rating:
|
Thanks for your advised. Tomorrow will go to try at site. |
Follow us on