2/24/2025 3:27 PM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi MindFlayer, It does not matter whether you are allowed to write to a certain path or not. This is because the WinCC Unified Runtime is executed as the service user "WCCILScsService". Please refer to the manual for details: It must be ensured that the "WCCILScsService" service user under which Runtime is running has read and write rights to the directory in which the logs are stored. Kind regards |
This contribution was helpful to
1 thankful Users |
2/25/2025 10:21 AM | |
Joined: 11/13/2018 Last visit: 8/28/2025 Posts: 91 Rating:
|
Hi Stefan Arcularius, Thank you for your response. Now it's clear! |
Like it? Rate it! |
|
Follow us on