3/4/2021 7:09 AM | |
Posts: 1 Rating:
|
Hello Guys, I have some problem with configuration ET200S COUNT module (138-4DA04-0AB0) to measure motor rotation speed . I connected the RPM sensor according to the diagram in the documentation: + 24V - terminal 6 sensor signal - terminal 5, ground - terminal 7. The direction of movement does not change and is not connected to the module. Сonfiguration parameters and current values from the counter module are shown in the screenshots. The problem is that the readings are randomly changing, including the movement direction. Please help me what I did wrong ------------------------------------------------------------------------------------------ |
Last edited by: ROnD1k at: 03/04/2021 07:56:17Last edited by: Jen_Moderator at: 03/04/2021 10:35:37New subject after splitting Last edited by: ROnD1k at: 03/04/2021 10:54:22 |
|
Follow us on