12/28/2012 10:28 AM | |
Joined: 1/27/2010 Last visit: 10/4/2022 Posts: 16 Rating:
|
Dear sir, I am working on a second-hand wire driwing machine , equipped with simens Simoverts and T400 technolgy Module. All the PLC and Drives are from Siemens. Because of some difficulties , the PLC and its components are disapeared from Switch-Cabinet and I bought new PLC (S7-400) and relatated component for the Switch cabinet and I intend to write PLC program for starting of the machine. In Hardware configuration of programm , I am not sure my design is correct , So I attached my program , if it is possible for you ,check my design and if it is necessary to correct , please send the corrected file for me. A-The Chassis type Simovert has following equipment : Simovert master Drive : 6SE7031-2EF20 (VC) Equipped with Electronic Box with following Items : - CUVC : 6SE7090-0XX84-0AB0 - ADB : 6SE7090-0XX84-0KA0 - LBA : 6SE7090-0XX84-4HA0 - CBP : 6SE7090-0XX84-0FF0 - T400 : 6DD1 606-0AD0 I guess the T400 module is programmed with SPW420 software for drawing machine , and it in not need , I edit programm with CFC software. B- The PLC S7-400 equipped with ETB module and I/O, following list : -PS407 10A : 6ES7 407-0KA01-0AA0 -CPU 414-3 DP : 6ES7 414-3XJ00-0AB0 -IF 964-DP : 6ES7 964-2AA01-0AB0 -DI 32XDC 24V : 6ES7 421-1BL01-0AA0 2 sets -DO32XDC 24V: 6ES7 422-1BL00-0AA0 2 sets -ETB 24DI/8DO : 6ES7 133-0BN0-0XB0 2sets -ETB 16 DO : 6ES7 132-0BH0-0XB0 -ETB 4/8 AI : 6ES7 134-0KH00-0XB0 2sets With best regards Farzad Taheri www.cnckaran.net Attachment2013-Hap.zip (371 Downloads) |
Follow us on