2/14/2022 2:58 PM | |
Joined: 9/27/2006 Last visit: 9/4/2025 Posts: 12397 Rating:
|
Hello pioneros; Can you identify the make and model of the Profibus slave in the upload of your PLC program more precisely? At first glance, a likely site for your gsd file search would be this one: https://www.hbm.com/en/1256/software-and-firmware-downloads-for-industrial-amplifiers/ They propose various weigh instruments and signal amplifiers that are Profibus-enabled, cjheck if your slave corresponds t one of these. For example in the site above there are at least 2 Clipx amplifier Profibus slaves in the list, knowing if this is one you need would make your search easier. As it is, simply register on the site and open the available Profibus gsd files to locate the one you are looking for. Ask HBM support for help if the file is for an older module, they should have your gsd file version in their archives. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 02/14/2022 16:00:03 |
|
2/15/2022 6:45 AM | |
Joined: 3/29/2017 Last visit: 7/23/2024 Posts: 16 Rating:
|
Here is a converter. It's probably the problem. It turns out you need to look for a file .GSD on this site? |
2/15/2022 7:15 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
GSD File can be found here https://www.hbm.com/en/2561/aed-digital-transducer-electronics/ you need a login for the download |
This contribution was helpful to
1 thankful Users |
2/17/2022 1:43 PM | |
Joined: 3/29/2017 Last visit: 7/23/2024 Posts: 16 Rating:
|
Thanks everyone for the help |
Follow us on