9/27/2021 8:04 AM | |
Joined: 6/26/2008 Last visit: 8/20/2025 Posts: 263 Rating:
|
What kind of third party applications do you mean? If you know, perhaps, you access to the WinCC Unified Runtime via a HTML5-Browser (e.g. Chrome, Firefos, Microsoft Edge, ...). If the "third party program" is a webserver, you can open it in the browser-control. Regarding the systemfunction "StartProgram" please keep in mind (see Manual): "On a SIMATIC Unified PC, this system function can only be used to start applications that do not have a user interface." This is a wanted behaviour. As I have heard you might can cheat this by calling a command-line program and open there an external program. But in this case you don't have an integration in the runtime. It will be external. |
1/20/2022 1:53 PM | |
Joined: 8/23/2012 Last visit: 7/15/2025 Posts: 15 Rating:
|
Hello, @BBritten, Could you please explain more what is "applications that do not have a user interface"? Thank you. |
Follow us on