2/10/2019 5:25 PM | |
Joined: 12/18/2014 Last visit: 9/8/2025 Posts: 35934 Rating:
|
All I can say is that this is not the case with me, but the way I wrote it in my first answer. |
2/10/2019 6:17 PM | |
Joined: 12/18/2014 Last visit: 9/8/2025 Posts: 35934 Rating:
|
I simply created a network project. The devices are the LOGO! 8.FS4 and an S7-compatible device. Then use the cursor to draw the connection between LOGO! 8.FS4 and the S7-compatible device, starting from the LOGO !. This will make the LOGO! set as client. AttachmentNetwork_project.wmv (309 Downloads) |
Follow us on