5/13/2010 1:10 PM | |
Posts: 27 Rating:
|
Hi, Does anyone have a sample code of communications between the s71200 and micromaster 420 using the USS Protocol ? i have checked the link above with 4 drives and motor but it is very complex for a beginner. your help is very appreciated Regards Aminadra Splitted from USS library and PKW Words. |
Last edited by: O_Moderator at: 5/14/2010 11:07 AMnew subject after splitting |
|
5/14/2010 12:20 PM | |
Joined: 9/23/2005 Last visit: 9/3/2025 Posts: 4416 Rating:
|
Hi, maybe, with adaptations, these Application & Tools could helps you: http://support.automation.siemens.com/BR/view/pt/40157517 |
Denilson Pegaia |
|
6/15/2010 8:06 PM | |
Posts: 126 Rating:
|
Did you ever get USS up and running properly? |
6/18/2010 8:48 PM | |
Posts: 27 Rating:
|
Hello, Below is the code for communication between S7-1200 and MM420 it is in pdf format as i was unable to upload the code in any way Regards Aminadra AttachmentS7-1200-USS.pdf (2822 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on