9/7/2021 11:24 PM | |
Joined: 7/13/2021 Last visit: 8/13/2025 Posts: 1 Rating:
|
Hi, I really appreciate the info. I just wanted to know if its possible to run applications of WinCC Unified PC Station in a PC where its WinCC V7.5 also installed additionally with the option of WebUX. I have installed Tia Portal Step 7 pro with WinCC Advanced/Unified V16 and WinCC V7.5 SP1 in the same PC and I have no issues regarding to the engineering, actually y can load the wincc unified runtime project and it seems to be running, however when I try to access the application via webrowser it only points to webux. Thank you. |
Follow us on