7/3/2012 1:42 PM | |
Posts: 3 Rating:
|
wat the purpose ppo |
7/3/2012 4:43 PM | |
Joined: 9/27/2006 Last visit: 9/9/2025 Posts: 12402 Rating:
|
Hello vijayarajan; The following FAQ describes PPOx (x = 1 to 5 for Siemens dtives) as part of the Profidrive standard. Which terminology do you use for cyclic PROFIdrive communication? PPOx allows the programmer to select the size and contents of the standard telegram to be exchanged cyclicallyover Profibus (now also over Profinet) between the pLC and the drive. The FAQ contains more detailed information on the subject. Hope this helps, Daniel Chartier |
7/12/2012 9:09 PM | |
Posts: 3 Rating:
|
sir just am using ppo 4 telegram i know that pzd 1-control word 1& status wordpzd 2,3,4,5,6 for whatwhere i have to give set point i need position control |
Follow us on