2/3/2012 10:49 PM | |
Posts: 8 Rating:
|
Hello All, I whant controll the step motor and I have small problem with axis configuration. I use CPU 1212C AC/DC/RLY and signal board SB1222 DC200kHz DQ 4x24VDC. I added and configured the technological object "Axis" and I have everywhere green points. I configured CPU, I added the SB and set puls and direction output on signal board - PTO Q4.0 Q4.1. I don't have program, I whant use control panel in CPU. When I run the panel, I have a message - axis is error, and - Parameter settings of pulse generator (PTO) are invalied (Address is invalied). I checked the address PTO in CPU and in technological object and are the same. Please help me, what I do wrong? Sorry for my English. AttachmentScreens.zip (562 Downloads) |
2/6/2012 12:40 PM | |
Posts: 267 Rating:
|
Hello, could it be that you haven't enable the pulse generator? |
2/6/2012 5:16 PM | |
Joined: 8/31/2010 Last visit: 7/18/2025 Posts: 1525 Rating:
|
Hello Przemos169, Refer Chapter - Motion Control is easy in this S7-1200 Easy Book Manual the same online version from here - Motion Control is easy |
Like it? Rate it! |
|
2/9/2012 10:25 AM | |
Posts: 45 Rating:
|
Hello I found this attachment when I was praticing motion control. you could also check utube there was once a video I think by bloodycow on how to configuring axis for motion control just search for s7 1200 motion. Hope This Helps Tom AttachmentPTO Motion Control.zip (667 Downloads) |
Last edited by: primus 1 at: 2/9/2012 10:44 AM |
|
This contribution was helpful to
2 thankful Users |
2/11/2012 12:21 PM | |
Joined: 8/31/2010 Last visit: 7/18/2025 Posts: 1525 Rating:
|
For motion control with S7-1200, refer these - it may help you Controlled positioning with S7-1200 via pulse/direction interface (CE-X7) Which Motion Control functions are there in STEP 7 (TIA Portal) V11 and how do you use these functions? |
Like it? Rate it! |
|
This contribution was helpful to
2 thankful Users |
1/7/2016 12:49 PM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
New question published by jowey is split to a separate thread with the subject error try to commission axis in manual mode . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on