11/24/2019 3:42 PM | |
Joined: 12/18/2014 Last visit: 9/9/2025 Posts: 35938 Rating:
|
Hello SELOGO, at first welcome to the forum. Was the IP address of your PC 2 years ago also 10.10.10.10? Which subnet mask have the PC and the LOGO !? Did you buy the other two LOGO!s now? If so, they will have different order numbers. And you can upgrade to the latest LSC version for free. LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) It is, however, a complete package with the size of 1.3 GB. After the download you have to install the upgrade as Administrator. |
Follow us on