12/5/2019 5:57 AM | |
Joined: 12/18/2014 Last visit: 9/5/2025 Posts: 35925 Rating:
|
In attachment a screen video and the related project. It explains how to manually create a connection between 2 LOGO!s. It is a client/server connection. AttachmentExample.zip (278 Downloads) |
This contribution was helpful to
1 thankful Users |
12/6/2019 5:43 AM | |
Joined: 12/18/2014 Last visit: 9/5/2025 Posts: 35925 Rating:
|
Since I can only answer you, what the manual says. The LOGO! can max. Manage 16 connections, of which a maximum of 8 connections can be static. Static connections allocate fixed resources. For dynamic not. See attachement. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 pages 29-31.pdf (307 Downloads) |
Last edited by: ixo65 at: 12/06/2019 05:43:34 |
|
This contribution was helpful to
1 thankful Users |
12/8/2019 7:55 PM | |
Joined: 10/1/2018 Last visit: 7/10/2022 Posts: 66 Rating:
|
At some point, when writing a program, BM KOU (see screenshot) got an incorrect connection. The program does not have NI and NQ for it. The program is working fine. But one static connection is uselessly busy. How to remove it?
Attachmentkou_kum_148 pwd nova.zip (257 Downloads) |
12/8/2019 8:32 PM | |
Joined: 12/18/2014 Last visit: 9/5/2025 Posts: 35925 Rating:
|
Your project has irreparable errors for us normal users. I have exported KOU program as a single diagram and then greyed out connections under Ethernet connections. That's not normal. Recently we had in the German-speaking part of the forum also such a problem. The solution in the case was: And again, a project where connections were created by drag & drop. |
Follow us on