3/25/2020 8:29 AM | |
Joined: 7/28/2017 Last visit: 4/11/2025 Posts: 4 Rating:
|
Hello Together I tried to get the log-file over the webserver, but it doesn't work. On the CD-Card i have insert with a card reader in the file webroot/main.html following download strings:
Back in the LOGO, I pressed on the webbrowser these download link, i get following error message:
So i think that it is not allowed to access the root directory. The other way is, to copy these main.htm to the root directory of the SD-Card and open the file in the browser "http://lfs/sdcard/main.htm". But i get the same error-message. The third way is, to copy the csv-files from the root to the webroot directory and get them on this place over the download link. But i don't know what i can use to do the copy. The easiest way were, that siemens changed their next logo update, to allow the download over http. Greatings ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/25/2020 11:06:45New subject after splitting |
|
Follow us on