8/24/2016 3:38 PM | |
Joined: 10/14/2012 Last visit: 9/9/2025 Posts: 10 Rating:
|
I am having system with Siemens TIA portal V12 and Simatic Step 7 software installed. Recently i tried to install microwin. Installation is happening whereas in PG/PC interface I am not able to find access point for microwin. I guess PG/PC interface is conflicting with one of the above installed software. How to solve this problem. I am getting an error if i try to set PG/PC interface "Specified access point not found". Note: I have installed the microwin in another windows7 64 bit system. During installtion, I got an error but after updating to SP9, it is working fine. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/24/2016 4:36:07 PMNew subject after splitting |
|
This contribution was helpful to
2 thankful Users |
8/25/2016 7:24 AM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, look to this topic, there is also batch that make update PG interfaces on Win7 x64. MICROWIN 4.0.9.25 INSTALLATION PROBLEM |
With best regards... |
|
This contribution was helpful to
1 thankful Users |
Follow us on