10/13/2010 11:08 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating:
|
Hi Do you require a limiter, you can write your own block for the same, Have fun.. |
Jazz |
|
10/13/2010 2:41 PM | ||||
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12396 Rating:
|
Hello hdhosseiny; The functions you describe can be found as part of the Modular PID package for Step 7: 2.1.23 ROC_LIM: Rate of Change Limiter Functional Description The block limits the rate of change of an output value. A step change becomes a ramp function. Two ramps (rising and falling values) in the positive and negative range can be selected for input variable and output variable. Control inputs set the following modes: • Default output variable • Tracking • Stepless automatic-manual switchover The value of the output variable can be limited by two selectable limits. If the rate of change limit rising or falling is reached or the high/low limit is reached, this is indicated at outputs. Extracted from: Modular PID Control manual http://support.automation.siemens.com/WW/view/en/1137082 More documentation:
Hope this helps, Daniel Chartier |
|||
Last edited by: dchartier at: 10/13/2010 2:43 PM |
||||
This contribution was helpful to
1 thankful Users |
Follow us on