3/19/2020 1:22 PM | |
Joined: 12/18/2014 Last visit: 9/7/2025 Posts: 35933 Rating:
|
For me is not clear what you mean with DCS System? Can you give more infos? |
3/19/2020 1:33 PM | |
Joined: 5/17/2017 Last visit: 12/20/2020 Posts: 64 Rating:
|
I have wrote it up their it is Modbus TCP/IP |
3/19/2020 1:54 PM | |
Joined: 5/17/2017 Last visit: 12/20/2020 Posts: 64 Rating:
|
Yes I have the latest LOGO! 8 :) All what I have is an IP address and Ethernet cable connected to my LOGO! |
3/19/2020 1:58 PM | |
Joined: 12/18/2014 Last visit: 9/7/2025 Posts: 35933 Rating:
|
Who is server, who is client? You have no type of the DCS System? No more Infos? |
3/19/2020 2:20 PM | |
Joined: 9/27/2006 Last visit: 9/7/2025 Posts: 12401 Rating:
|
Hello hasham; You initiated this conversation, and you are the one asking for help. ixo65 is trying to help you, and you are being difficult answering very basic questions about your system. What is the problem? Are you working with a Yokogawa Centum DCS for example? If yes, do you have a DCSX3000 module (Modbus TCP and serial) mounted as a communication processor? How is it setup, in the case you can answer yes? https://web-material3.yokogawa.com/IM39J06B40-02E_1.us.pdf If you do not take this seriously, our expert in Logo! ixo65 will lose interest in your question. Hope this helps, |
This contribution was helpful to
1 thankful Users |
Follow us on