3/1/2021 12:01 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello AzzabiRiadh11, if you re-import the GSD file for NPBA-1 from ABB into HWKonfig, you have to update the module catalog. If the project planning of the NPBA-1 already exists and you have imported a new version of the GSD file, you must update the GSD file (for the project planning. Also check whether the addressing of the inputs and outputs is still correct. Then save and compile and perform the download. https://new.abb.com/products/de/58919454/profibus-adapter-npba-01-option-sp With best regards |
This contribution was helpful to
1 thankful Users |
Follow us on