7/16/2020 7:00 PM | |
Posts: 3 Rating:
|
Dear vipz, I would appreciate if you could help me, I have a project similar than yours. In summary the project is about communicate a S7-1200 with PROFIBUS slave module 1242-5 with a PROFIBUS master of Schneider M580. My job is just the configuration of the Siemens slave, I won't have to deal with the master. I just have to send the gsd of the CM 1242-5 to the master manager. I need to confirm if the complete configuration in the slave side is: - Insert the address : (in my knowledge is not possible to assign the subred in Tia Portal because the master is 3rd party(schneider)) - Fill the transfer area with the registers that have the data of interest: (in my knowledge is not possible to assign the DP Master in Tia Portal because the master is 3rd party(schneider)) Or there are some other things to do in the slave side? Hope hear from you soon. Regards. ------------------------------------------------------------------------------------------ |
Last edited by: Benshapp at: 07/16/2020 19:01:16Last edited by: Jen_Moderator at: 07/17/2020 06:17:01New subject after splitting |
|
7/16/2020 8:15 PM | |
Posts: 3 Rating:
|
Hi Duris, Sorry, my mistake. Attached I leave the images. Attachmentimages.zip (414 Downloads) |
Follow us on