1/10/2012 11:17 AM | |
Posts: 13 Rating:
|
Dear, |
1/10/2012 5:53 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi, the "Timing Diagram" version for Simovert Masterdrives does not exist, however, the only State Diagram is in the Function Diagrams Page 520 of the Compendium. Regards, Graeme |
1/10/2012 7:47 PM | |
Posts: 13 Rating:
|
Thanksfor answer, Graeme. I already knew about this diagram. It has disadvantage: it shows transitions between internal states of VFD, but there is no information, how VFD states are associated with status word bits. I suppose, the only way to clarify a behavior of VFD status word bits is experiment. |
4/29/2012 11:48 PM | |
Joined: 7/8/2009 Last visit: 6/7/2025 Posts: 1977 Rating:
|
Whats the problem there? Status bits looking normal after Run command If you worried about changing from 4331 to 5334, then its natural due to change in some bits after drive run have a look at attached status word bits Regards Devesh Vithani AttachmentSW1.pdf (440 Downloads) |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to
1 thankful Users |
Follow us on