1/3/2022 5:40 AM | |
Joined: 10/25/2021 Last visit: 5/8/2022 Posts: 1 Rating:
|
hi expert I have a CPU S7-315, communicated via Profibus with six drives three of them Danfoss and the rest three are Sinamics G120C the Sinamics drives a three fans in the sterilization Tunnel of critical area which mean no way to turn off any of these fans. the problem is duo to any losses of communication the sinamics drives stop. so I am looking for any configuration/parameters of the sinamics drives to let the drive run even if the communication is interrupted as a reference operation, if no connection the drive run with base speed . i hope to find a solution for this issue. thank you in advance Expert. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 01/03/2022 10:41:56New subject after splitting |
|
Follow us on