6/13/2011 10:43 AM | |
Posts: 1 Rating:
|
Dear collegues, I have a problem at MC drive 6SE7021-0EP70-Z. That convereter drives a 1FW3150 serie torque motor which coupling with a roll. The problem is while line is running with 500m/s, because of the process requiriment another roll get pressed to it, and at that time MC convereter output frequency is reducing and roll speed becames nearly 200-250m/s. This speed reduction directly effects the production quality. It might be torque limitation which cause the reduction of output frequency of the MC drive. How can I solve that unwanted speed variation. Parameter file of MC Drive is at the attachment for your opinion. Regards AttachmentMC.zip (287 Downloads) |
Follow us on