11/19/2024 6:51 PM | |
Joined: 11/18/2024 Last visit: 2/11/2025 Posts: 1 Rating:
|
Hi, I have the S7-1500 1516F-3 PN/DP (6ES7 516-3FN02-0AB0) and I want to use it with Openness API. In TiaPortal I have buttons for "start CPU" and "stop CPU" and I want to do that in a C# program using OpennessAPI. In the official documentation in chapter 5.11.1.8 there are code examples that show how this is accomplished, but it seems like it's only possible before and after a download. Is it also possible to start and stop the CPU without doing a download? I am asking, because when I want to do the download, I get an exeption that says "Loading or overloading fail-safe data in Openness is not permitted." (or in German: "Laden oder Überladen fehlersicherer Daten mit Openness ist nicht erlaubt."). According to this thread: Loading or overloading fail-safe data in Openness is not permitted. - 257894 - Industry Support Siemens , it seems like I can't download the project into my device at all. Am I right? So does that mean, I can't start or stop the CPU via OpennessAPI? |
Last edited by: MichaelDeSanta at: 11/19/2024 21:39:11 |
|
Follow us on