10/1/2021 11:54 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
https://support.industry.siemens.com/cs/de/en/view/109782287 Site 776 |
10/1/2021 12:00 PM | |
Joined: 4/28/2015 Last visit: 5/16/2025 Posts: 1278 Rating:
|
And here you can also find a ready to use SIMATIC FB to control a SINAMICS drive via Tel 352. LSinaExt with the SINA_SPEED_TLG352 block: https://support.industry.siemens.com/cs/de/en/view/109747655 |
Best regards, |
|
10/4/2021 7:49 AM | |
Joined: 9/30/2016 Last visit: 8/13/2025 Posts: 946 Rating:
|
Hi RB91, Thank you for answering. I do however not see where I can see the actual torque (or actual current) in the examples you are giving the links to. I don't need to control the position or do homing - it is a simple motor control where I need the actual torque in the PLC - so I want to know the address of this value in the status word when using telegram 352. I am not sure they have used the block "SINA_SPEED_TLG352 (FB38004)" in the application but will the torque still be in PZD4 - USER2 - MIST_ GLATT as in Table 2-8 on page 14 as long at the telegram is 352? I don't really understand "Table 2-10 Reference values input parameters" - why is it necessary for the drive to get reference values (setpoints) to tell us the actual values?
|
10/4/2021 9:51 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
PZD4 = 4th word in the telegram, so 4 is the offset |
Follow us on